This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM76005: WeBench error correction request about SYNC/MODE conection for FPWM

Part Number: LM76005

Hello,


My customer using LM76005 for the following requirements.
  Vin=36V
  Vo=5V
  Iout(max)=3A
  FPWM mode
Based on WeBench, they tied SYNC/MODE to VIN.
But, since SYNC/MODE is logic input and its absolute maximum voltage is 5.5V, much less than Vin=36V, LM76005 was broken due to this error.
Please correct the WeBench at next update timing.

Best regards,

K.Hirano