Hi,
In the circuit I created with the BQ24610, although I only connect the adapter and not connect the battery, the STAT1 led is on and the STAT2 led is off. When I connect the battery, the STAT1 led remains on, while the STAT2 led remains off. While the battery is connected, the battery is not charged in any way and no charging current is generated.
As a result of my general research on the circuit, I saw that the VMax value at 3.21 Volt in the wave I obtained from the PH node was not at the desired value when there was only the adapter voltage in the circuit. You can find the sample PH node wave.