This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25947: Protection Circuitry

Part Number: TPS25947

Hello,

We are using the TPS25947 and had some questions about protection circuitry. See Figure 10-1 below taken from the datasheet.

Our application:

VIN = 5V0

Iout = 1.5A peak - should theoretically be much lower

Questions:

In what case do we need D3 and D4? This section in the datasheet mentions 20V USB interface. Do you think it is applicable to our application? 

D2 is a Schottky diode used for negative transients. How should we spec this diode? Current rating? Forward voltage? Would something like the MBR1H100SFT3G be okay?