Hi,
We have simulated TPS544C25 in WEBENCH Power Designer with below Specifications:
VinMin = 10.0V
VinMax = 12.5V
Vout = 5.0V
Vout Sch = 5.0V
Iout = 5.19A
With WEBENCH Results, all the parameters looks fine and it meets all our requirements. When the same circuit with same specifications is simulated in PSPICE for TI Tool, it is giving error; Phase margin is not meeting.
With WEBENCH Power designer, the Phase margin shows Phase Marg 47.956 deg. But when we run the same in PSPICE, Phase margin was showing 36 deg.
/resized-image/__size/320x240/__key/communityserver-discussions-components-files/196/TPS544.JPG
Please Clarify, which simulation we need to consider. Which one is most relabel.
Thanks & Regards,
Ramakrishna D C
Logic Fruit Technologies Pvt. Ltd.