This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A66-Q1: Bode Plot Measurement

Part Number: TPS7A66-Q1

Hello Team,

is it possible to do a Bode Plot measurement on a TPS7A66-Q1?

Because there is no feedback pin to inject the signals.

Many Thanks

Josef

  • Hello Josef,

                       At this point we do not have a method to make Bode plot measurements for phase margin information with the device on a board/ EVM. Even if the FB was available to break the outer loop, the LDO design consists of other multiple internal loops which cannot be accessed or broken. 

                       The response of the LDO to a quick load transient is an indirect but an effective method to asses phase margin and stability. Here is a link to an app note that further describes this: https://www.ti.com/lit/an/slva381b/slva381b.pdf. Thanks!

    Regards,

    Srikanth