This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A03: Alternative

Part Number: TPS7A03


Hi,

Good Day.

Customer is trying to find an alternate for TPS7A0318PDQNR with active low enable logic.

Kindly let us know if there is any alternative for TPS7A0318PDQNR.

Below are the key requirements:

1. Output voltage: 1.8V, Single, Fixed

2. Package: 4-X2SON (4-XDFN Exposed Pad) 

3. Active low enable logic

4. Low quiescent current

Please advise. Thank you very much.

Best Regards,

Ray Vincent

  • Hey Ray, 

    Good day. Unfortunately, we do not have any parts that are X2SON with active low. We would recommend using the TPS7A03 and using an inverter. But another option, could be using theTPS76918DBVR as this active low EN, but it is in a SOT-23 package instead (comparison below). 

    Let me know if you have any additional questions. 

    Thanks, 

    McKyla