Hi Expert,
My customer is testing TPS22919 behavior at over load situation with e-load.
When the output current is increased with e-load. TPS22919 was shutdown at Iout = 2.9A.
At this time, Vin- Vout < 1.5V, Vout > Vsc. However the device seems to be shutdown state
Is it thermal shutdown? (The package temp is 93C)
Then they decreased output current slowly.
The device restarted at Iout <100mA. (They tried to check a few times, always around 100mA. Not shutdown when they keep 200mA setting)
They think, it is not thermal hysterisis. Does the device have any restart condition other than thermal hysterisis?
Thanks
Mukuno