Other Parts Discussed in Thread: TPS65132, , USB2ANY
Dear TI,
I found below description in tps65132xx datasheet. It said that for tps65132A, pulling both ENP,ENN low will disable the device but the I2C can still communicate with tps65132A.
My question is for tps65132S, if the only EN pin is pulled down, is I2C of tps65132s still accessible?
If the answer is NO. Does it mean that I have to pull EN pin high firstly and than write the configurable registers like reg0x01,02 for positive and negative output voltage, and reg 0x02, reg03 for the power-on and power-down sequence control?
If my understanding is right, it seems a little strange for me, because if EN pin is pulled high, Vpos and Vneg will have outputs immediately without delay as the default value of reg0x02 and 0x03 configs. Then we can not realize the power-on sequence and delay time we want. I doesn't make sense.
But when I pull EN pin low on tps65132S EVM, I cannot connect to the it with USB2ANY tool and GUI.
Look forward to your feedbacks, thanks.