I have a couple of questions for LMR43620mSC3RPERQ1 design
- I checked the datasheet (revised in Dec 2021), for reference voltage setup (Pin Vout-FB), the suggestion value for Rfbt and Rfbb is shown below
- I used WEbench power design tool, it gave me different configuration below.

- I found another datasheet which was revised in Oct 2021. I found 100K vs 43.2K configuration.

- I want to know which one is correct configuration for the Rfbt and Rfbb?
- For the two datasheet, I noticed that there are difference on Rent and Renb design (External UVLO) . Which one is correct one?
- I noticed there is different between the table 9-1. The older version has 1000KHz column, but the latest one does not .
I also want to know if the input filter, caps and output inductor selected via Webench design match the chip or not. I mean if I can use the design from Webench directlu?
Thank you.