Hello all,
I'm just curious about the series resistor in the 10 input pin. Why in some parts of the datasheet of the UC3525 is shower a 3K, and in others you can see a 5K resistor? Could be a mistake?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello all,
I'm just curious about the series resistor in the 10 input pin. Why in some parts of the datasheet of the UC3525 is shower a 3K, and in others you can see a 5K resistor? Could be a mistake?
Thanks!
Andres,
I see two examples in the UCC3525A data sheet block diagrams that are showing 3 kΩ internally connected to pin 10 (shutdown) and one example showing 5 kΩ (Fig 5). You are correct that this is most likely a typo in the Fig 5 example. In either case, the internal resistor is simply limiting the base current to the internal NPN shutdown transistor. The internal value of this resistor will have no impact on external component selection since it is recommended to pull pin 10 high (~1V<V<5V) for shutdown. Thanks for connecting through E2E and bringing this to our attention.
Regards,
Steve M