Hi ,
We are using TPS54318RTER in our design to generate 1.8V & 3.3V . Both are power from 5V input supply. As per the datasheet, we have adjusted the Vstart and Vstop for both output voltages with a resistor divider on EN pin.\
- Rtop= 10K , Rbottom = 4.3K
With above resistor values, we would get Vstop = 3.892V & Vstart= 4.124V. But this configuration the boards not at all booting. The current drawn by the board is typically 1.37A, when board is not booting.
When we change the values of Rtop & Rbottom,( As per the datasheet , 133K & 105K respectively), the board is working perfectly fine. The current drawn would go up to 1.67A (Normal).
What would be the cause for the issue? Could you please help us.