Hello,
We have a problem with OTG mode of BQ25892. All features of chip are working correctly beside the fact that we are unable to set OTG_CONFIG bit while chip is power supplied via VBUS. After having OTG_CONFIG bit set over I2C it is read back as 0. Problem only exists while charger is power supplied over VBUS, after having VBUS disconnected we are able to set correctly OTG_CONFIG and it keeps it's correct state even after VBUS power returns. After having it set to 0 we are unable to set it again while VBUS is present.
Problem seems to be the same as:
Many thanks,
Krzysztof