This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Team,
I am looking at the TSP783 product package to understand the different P2P drop-in possible alternatives.
Can you please help me to confirm/understand the below?
-Just looking at the package geometry: Can SOT-23 |5 be used in place of a SOT-23-THIN | 5 package on an existing PCB without rework?
There seems to be some mismatch in the package information displayed for the compatibility (see pink highlights in TI.COM screenshot below).
-Can you double check?
Thanks in advance,
A.
Hi,
The main difference between both packages is the height.
Also one of the reasons why TPS7A24 shows as different pinout, is because, Pin 4 is either FB or NC as TPS738 is GND. If you are going to use a fixed version then there would be no trouble. As for the others, since Pin 4 is NC, therefore they are drop in replacement.
I will get the information fixed on our end regarding the dimensions.
Best,
Edgar Acosta