Other Parts Discussed in Thread: TPS61021A, TPS61022, LM2623
Dear Sir/Ms.
We promote TPS61023 for 3V Mercury battery input solution.
My customer RD Now is considering AAA*2 and AA*2 battery input. TPS61023 start up voltage is 1.7V.
Following specifications PM and I double check with RD.
Vin 1V~3V (Target 0.8V~3V) , (Start up voltage)
Vout=3.3V, Max. Iout=0.3A.
Not Request QFN Package. Customers want SOT's packaging (with legs) in order to facilitate maintenance.
I can not find Products that meet the price advantage and meet the specifications.
Is there any new boost IC that meets the customer's specifications?
Best Regards,
Kami Huang