Other Parts Discussed in Thread: LM5010
Hello,
I face a problem with the LM5010. My circuit turns it on by asserting the RON_SD to '1' after the input voltage crosses 50V. It is configured for 32V output (Data sheet resistors are set to R1=12K, R2=1K, No R3).
After the component is turned on and active for 40ms, it is shutdown by asserting the RON_SD pin to low for approx. 5ms causing the component to shutdown (this is because the input voltage drops down for a while). Refer to the attached drawing.
After 5ms the RON_SD is turned high again (and remains high forever), but still the component continues its shutdown process for approx. 150ms before it is turned on again. According to the data sheet, the shutdown time shall be approx. 1uS.
The RON resistor is set to 100Kohm.
During first activation, there is no load (only R1 & R2). Later in the process a load is connected (by turning on a transistor). The load is connected after approx. 100ms into the shut down process.
Is that a normal behavior?
If not, what could explain such a behavior?
Thanks a lot,
Ilan