This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53317A: Frequency tolerance checking

Part Number: TPS53317A

Hi All,

May I know what is the frequency tolerance under 1.2V input, 0.6V output, 2.7A Iout, and 600kHz setting?

It hard to judge based on the below figure from the datasheet.

The customer request +/-10% means 540KHz~660kHz but the testing result is 670kHz.

May I know whether it is acceptable?

Thank you all.