Other Parts Discussed in Thread: BQ25798
(Please refer to the related topic for project information)
When the VBAT is very low the BQ starts the charge in the TRICKLE CHARGE mode. At this moment the VSYS is 8.88 V, below the VSYSMIN = 9.0 V and the status of VSYS is "In Regulation" (REG1E_Charger_Status_3 Register - bit4).
This condition causes the shutdown of the system and we can't see the status of registers after this problem. Is it possible that the BQ is cutting-off the VSYS in the TRICKLE CHARGE?
Similarly, it also happens if you don't have a battery connected, in this case the VSYS = 9.27V and NOT CHARGING status but the system still shuts down completely.
Register/Description |
Value |
---|---|
REG20_FAULT_Status_0 |
0x00 |
REG21_FAULT_Status_1 |
0x00 |
REG1B_Charger_Status_0 |
0x0F |
REG1C_Charger_Status_1 |
0x2A |
REG1D_Charger_Status_2 |
0x00 |
REG1E_Charger_Status_3 |
0x30 |
REG1F_Charger_Status_4 |
0x10 |
REG1C_Charger_Status_1.CHG_STAT |
Trickle Charge |
REG33_IBAT_ADC |
0 mA |
REG35_VBUS_ADC |
11.71 V |
REG37_VAC1_ADC |
11.71 V |
REG39_VAC2_ADC |
11.75 V |
REG3B_VBAT_ADC |
1.98 V |
REG3D_VSYS_ADC |
8.86 V |
REG1B_Charger_Status_0.VBUS_PRESENT_STAT |
1 |
REG1B_Charger_Status_0.AC1_PRESENT_STAT |
1 |
REG1B_Charger_Status_0.AC2_PRESENT_STAT |
1 |
REG1B_Charger_Status_0.POORSRC_STAT |
0 |
REG1E_Charger_Status_3.VSYS_STAT |
1 |
REG1F_Charger_Status_4.VBATOTG_LOW_STAT |
1 |