This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV840-Q1: Is there a 2.9V open drain version?

Part Number: TLV840-Q1
Other Parts Discussed in Thread: TPS3840

Hello,

The typical application circuit on the first page of the schematic of the TLV840-Q1 shows a part number of: TLV840MADL29Q1.

But the only 2.9V option that shows up in the ordering information on the product page is the TLV840MAPH29, which is a push-pull version. 

Also, on the product page it doesn't even show 2.9V as an option for the threshold voltage...

Is there an open-drain version of this part with a 2.9V threshold? If so, why doesn't it show up on the product page?

Thanks,
Daniel