Other Parts Discussed in Thread: BQ2980
Hello,
In the user guide it states I need two power supplies and one "with current source and sink to simulate a charging and discharging event."
Further down in the guide (Step 2.4.5) it claims I should have this ability to source and sink from both supplies from 100mA to 200 mA.
In various sections of the guide there are recommendations that, "When using a power supply for evaluation, be sure the power supply can accept or is protected from any reverse current such as with a blocking diode if another supply is used in the system."
I have three questions surrounding these requirements:
1.) If I have an external reverse current blocking diode on each supply, do I still need the supplies to handle sinking any current? These two recommendations (adding a diode and having sinking abilities) seem to be conflicting or maybe I am misunderstanding something.
2.) If I do in fact need a supply with sinking ability even with protection diodes, what is an example or recommended DC power supply for this? I'm not familiar with sinking abilities from supplies nor do I see any such spec on all bench supplies I've looked at.
3.) Why are the sink abilities only from 100mA to 200mA? Shouldn't we expect up to 8A as per the maximum of the board?
Best regards,
Christopher