Hi all,
We are trying to add a drop-in alternate to TPS79901-EP for purchasing timeline.
the idea is to select TPS73401DRVR as the alternate to TPS79901-EP.
the LDO is converting the 3.3V input to 1.50V output (max 150mA at output) to power a FPGA core.
as the FPGA core 1.5V voltage input is within 1.425 & 1.575, the drop-in replacement will move the nominal 1.5V power voltage from 1.50V to 1.52V which is an acceptable value for the FPGA core. the TPS73401 can source more current than TPS79901 (250mA) and LDO dropout is in the same order order of magnitude for the use case.
the only concern (except the temperature screening @-55°C must be done for the TPS73401DRVR as the use cas is within the military temperature range: -55°C to +125°C) is to verify the thermal features of TPS73401 and the TPS79901 are in the same order of magnitude.
Datasheet of TPS73401 indicates Junction to ambiant JθA (jedec High-K) of 65°C/W.
Datasheet of TPS79901-EP indicates Junction to ambiant JθA of 74.2°C/W but here there is no indication of jedec High-K/Low-K setup, therefore it is not clear to state whether TPS73401 JθA is better than TPS79901-EP JθA or not. Can someone provide clarification on thermal comparison between these 2 Parts ?
Many thanks,
Pascal