Other Parts Discussed in Thread: TLC59116
Hi support team.
I receive a inquiry from my customer regarding delay time.
Could you prove me the information about delay time from resister set to output applied?
Best Regards,
Higa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Higa-san,
Here is a test result for your reference. From sending commands to output active, it takes around 5ms.
Hi Wu-san
Thank you for sharing.
My customer would like to know your all register setting.
In particular, they interest whether the delay time does not change depending on the OCH setting of MODE2.
Could you provide that?
Best Regards,
Higa
Hi Higa-san,
The delay time would not change whether this bit is 0 or 1. When set as changed on ACK, the output would changed after the related register is written. When set as changed on Stop condition, if auto increment function is used, several registers are written together in the one I2C command and all outputs would changed together after stop condition sent. But the delay time is around 5ms no matter what the trigger point is.
Hi Wu-san
Thank you for your kind support.
I'm sorry for the additional request, but could you please provide the waveform data in the I2C sequence below?
This is a request from my customer.
1. PWM control (0x0A) 00h-> FFh-> 7F
2. Set the OCH bit in the MODE2 register to 0-> 1 and execute the No. 1 sequence.
The reason they asked is because they want to understand from the data that the delay time does not change under the following two conditions.
- Continuous PWM setting
- When OCH is changed from the default value "0" to "1"
Thanks and Best Regards,
HIga
Hi Higa-san,
Yes I can test it but I am out of office today. I will reply you in next Monday.
Hi Higa-san,
Sorry that I am out of office in business trip. The results will be replied for you in tomorrow.
Hi Higa-san,
Here is the test results for your reference.
The conclusions are:
1) OCH value does not influence the delay time significantly.
2) PWM value change vary from the work state:
>From off to on, the time is most long around 5ms;
>Changing the PWM setting in different value need around 1ms;
>Turning off the outputs will be valid immediately.
Hi Higa-san,
Sorry that it seems there are some issues happened on the scope that only one image was saved, which replaced others. The conclusion I observed could be used for communicate with customer firstly. For the bench waveforms, I can re-test for you later. But the covid epidemic situation is not optimistic at Shanghai and we all start work from home. The results will be sent to you maybe 2 or 3 weeks later. I think you customer could test it on TLC59116's EVM, which is 16-channel version of TLC59108 and have the same behaviors.
Hi Higa-san,
I will close this thread firstly. If there has further support, you could start another new thread or email me directly. Thanks.