This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28C45-Q1: active clamp for 800W Power level design?

Part Number: UCC28C45-Q1


Hello,

I have just got doubt whether can I use Active clamp topology in 800W to 1KW application?

All the literature says Active clamp forward can be used up to 500W.

Lets discuss in the forum what are consequences (pros & cons) if we use active clamp forward in 800W & 1KW application.

Specification:

1. Vin = 36V to 120V

2.Vout= 13.5V

3. POut= 400W,800W,1KW

4. Isolation = Yes

Hope for informative discussion.

Thanks & Regards

Nitesh Modi