This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Here's an issue form the customer may need your help:
The Bluetooth small system charge current is around 75 mA. The customer would like to confirm which of the BQ25175 and BQ2510X are the main recommended materials.
Also they want to know if the BQ25175 can be used for battery charging of 4.2 V.
Could you help check this case? Thanks.
Best Regards,
Cherry
Hi Cherry,
The customer can consider either the BQ25170 or the BQ25180 for 75mA charging current and 4.2V battery voltage. The BQ25175 has Battery regulation voltage of 4.35V.
Thank you.