I was looking at the BQ24075T for an application. It is very close to my needs but for a couple of things. I would like to know if this is the best option.
Requirements;
Single cell LiIon battery to be charged from USB (no AC power pak), Need to be able to select 100ma or 500ma current limit. Need to drrive system voltage at USB current levels while charging. System votlage requirements are; 4.9V to 5.2V. can the output voltage be adjusted.
I also would like to include a Fuel Cell function. Is there an integrated charger + power path managment + fuel cell?
Thanks,