This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am planning to use 5V for the TLV752 input.
For Vout_1 to be 3.3V, I am planning to use the following:
For Vout_2 to be 1.8V, I am planning to use the following:
Could you please confirm if these resistors values are okay to use to yield 3.3V and 1.8V at the outputs?
Thanks and best regards,
Seong
Hello Seong,
The voltage at the output pin is set by the equation VOUT = 0.55* (1 + (RFB TOP/RFB BOT)). With RFB TOP = 6KΩ and RFB BOT = 1KΩ , VOUT1 will not equal 3.3V. With RFB TOP = 2.48KΩ and RFB BOT = 750Ω VOUT2 will not equal 1.8V.
I recommend the following resistor values for VOUT = 3.3V : RFB TOP = 48.7KΩ and RFB BOT = 9.76KΩ. For VOUT = 1.8V : RFB TOP = 48.7KΩ and RFB BOT = 21.5KΩ. Thanks!
Regards,
Srikanth