Hi Team,
Our customer would like to generate an output voltage from 88V to 167V @ 75mA output current using the TL783 from an input voltage of 250V. Since the differential voltage exceeds the maximum Vi-Vo of 125V, he would like to know if he can put a series zener diode between the 250V source and the input of the TL783 to reduce the voltage by 50V. Will this work?
Regards,
Danilo