Part Number: REF3433-EP
Other Parts Discussed in Thread: REF35, , REF34
This voltage reference has an output capacitor spec of 0.1 to 10uF. The time from enable signal active to stable output voltage is specified as 2.5mS typical with 10uF output cap.
Looking at Fig 13 in the datasheet, one may conclude that lowering the output capacitor value would lower the "power up" time, probably proportionally to the output cap value.
For instance, if the output cap value were lowered to 0.1uF, would the power up time be reduced by a factor of 100 (25uS) ?
I have an ultra low current requirement for an MSP430 application where I want to keep the reference off until it's needed, but it needs to "power up" quickly. The micro would wake, turn on the reference, and must be ready to sample (use the reference) in less than 100uS.
Thanks.