Hi,
I would like to ask a question on TPS54310.
In Spectrumdigital’s EVM6437 schematics, I found that different inductor values (3.3uH and 2.7uH) are used for different output voltage (3.3V and 1.8V). Is there any particular reason for choosing such different values?
More specifically, is the correct value of inductor an exact value, or a range that any inductance falls within it could work? Could I used either 3.3uH or 2.7uH for both {3.3V and 1.8V} output?
Thanks,
Zheng