Part Number: TPS62827
Other Parts Discussed in Thread: TPS62826,
Hi there, we use the TPS62826 in our design but due to supply chain issues are fitting in the TPS62827 instead. Do we have to change anything in our design?
Looking at the EVM, it looks like the TPS62827 adds an additional 10uF of capacitance on the output. Is this to support to additional current capability of the device (4A) ? To my knowledge, there is practically no difference between the TPS62827 and TPS62826 besides the current limit.
Our applications max output current requirement is 2A peak.