Other Parts Discussed in Thread: TPS1653
Hello,
My name is Itamar.
My application is a wall adapter that should charge a Lithium-Ion battery with a CCCV profile.
The battery charge voltage (CV) should be the same as the wall adapter voltage (Voltage range is: 25-40V)
The battery charge current (CC) should be between 3-5A (adjustable).
The wall adapter is the single power supply for the system, it supplies the system needs and two battery chargers.
I look for TI current limiter IC that will be connected between the wall adapter and battery.
The current limiter IC should be set between 3-5A and should work continuously in current limit mode (the battery draws the maximum current that the source can give).
Application Block Diagram:

I will appreciate a quick response.
Thanks,
Itamar