This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6594-Q1: Maximum number of write cycles of internal NVM

Part Number: TPS6594-Q1

Dear Experts,

we want to use the GPIOs of the PMIC to remember beyond a power-cycle a binary state of the hardware platform, via programming the internal NVM (via I2C / SPI), to set the system during the next power-up in a defined state (depending on the programmed Bit / GPIO).

Could you please provide more detailed information to the internal NVM (technology, max. number of write cycles,...) of the referenced PMIC and give a feedback, if the above described use-case is possible?

Thank you!