The BQ500110 has a primary and alternate communication channel, is the alternate channel used for redundancy ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Ron,
Two channels of communication are redundant to each other. Some redundancy helps when secondary-side impedance-modulation communication excibits nulls of communication -- points at which amplitude of the signal received on the primary side drops to very low levels. It was experimantaly shown that having two channels with different detecting approach can help better resolve communication null problems. One of the channels is a peak-detector and another is a synchrronous detector.