This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23754: Confirm use of FET

Part Number: TPS23754

My customer is looking to use these 3 FETs with the TPS23754, is there any concern on these in terms of the TPS23754's ability to drive them properly?

MPN

FM100N60ADN

DG100N14Q

MTE013N10BRH8

Unit

Vgs

20

20

20

V

Vds

100

100

100

V

Vt

2.8

1.7

2

V

Id

60

54

35

A

Id(pulsed)

240

100

140

A

Qg

32

21.23

20

Rds(ON)

7.2

13.4

12.5

mohm

Nick

  • Hey Nick, 

    If these are going on the primary, I would suggest 150Vds rating. Otherwise there is no issue with driving these FETs. 

    If this post answers your question, please indicate so by marking this thread as resolved. Thank you.

     

    Regards, 

     

    Michael P.

    Applications Engineer

    Texas Instruments