Other Parts Discussed in Thread: TPS7B70-Q1
Hi expert,
My customer was using MAX25210 on their project now we would like to use our portfolio to fight against them.
Here are their features need:
1. LDO Output could be fixed 3.3V or 5V, or be adjustable output.
2. 5V undervoltage/overvoltage detection
3. The 5V overvoltage/undervoltage reset output delay time can be set.
4. Output capacity: Iout should be 300mA and above
Please refer to MAX25210 datasheet and promote us some proper devices for customer reference, thank you!