This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Minimum input capacitance for multi-module design

Other Parts Discussed in Thread: PTH05050W, PTH04000W

I have a design that has 3 power modules, PTH05050W and PTH04000W (x2).  These are feed by a common 5V main supply.

PTH05050W  - 5Vin, 3.3Vout, 3.0A max, step load 0.5A max

PTH04000W - 5Vin, 2.5V out, 1.0Amax, step load 0.30A max

PTH04000W - 5Vin, 1.2out, 1.5A max, step load 0.30A max

 

The data sheets call for input capacitor of 100uF, 47uF and 47uF minimum respectively.  It is desirable to keep capacitance to a minimum for size and inrush reasons.  According to appnote SLTA055, it seems that I "could" use less capacitance and meet my requirements.

http://focus.ti.com/analog/docs/litabsmultiplefilelist.tsp?literatureNumber=slta055&docCategoryId=1&familyId=561

Question - Can I safely use something less for input capacitors ? Concerns if I use less.

I currently have a 33uF tantulum and 10uF ceramic on each and everything seems OK.  I just need to clarify if this is or is not OK.

There are 4 cap pads per input (two large, two small) that can be used for other caps if you have a better recommendation.