To whom it may concern:
BQ34Z100-G1 is used on a 9S1P battery. During storage test, the IC is set to deep sleep mode, and several battery got increased SOC. The FCC looks OK. The worst case (18 weeks storage) SOC increased to 93% from 30%, and another (14 weeks storage) was 55% from 30%. Here is the log data after the storage.
Current(A) | Voltage(V) | StateOfCharge(%) |
0 | 31.96809 | 93 |
0 | 31.96793 | 93 |
-0.00085 | 31.36862 | 93 |
-0.05 | 31.94114 | 93 |
-0.05 | 31.94022 | 93 |
-0.05 | 31.9398 | 93 |
-0.05 | 31.94005 | 93 |
-0.05 | 31.93896 | 93 |
-0.05 | 31.93913 | 93 |
-0.05 | 31.93821 | 93 |
-0.05 | 31.93813 | 93 |
Obviously the voltage and SOC don't match. The 9S1P battery is set to charge to 37.8V, so 93% SOC should be over 36V.
This battery could be discharged, and at the end 27V (3V/cell), the SOC is still 70%. Then the battery was fully charged, and SOC reached 100% while before the CV mode. In the next discharging cycle, SOC was back to normal.
Here is the Pack Config C register: 0x33, so RSOC_HOLD is not enabled, and RELAX_SMOOTH_OK and SMOOTH are enabled.
Could you help to check the root cause of this SOC rising issue, and how should we set the configuration?
Thanks!
Chen