This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Aaron,
This is not specified for this device. Usually the current limit decreases with higher temperature, due to the higher Rdson of the sensing FET. This also matches with the D/S values that show a lower current limit at lower Vout (which have a lower efficiency, meaning higher thermal losses).
Let me know if you havce any further questions.
Thanks,
Dorian
Hi Dorian Brillet de Cande
1.Your diagram is low-side FET vs high-side FET
Am I misunderstanding?
2.Yes, my experience is also that the limit current decreases when the temperature is high. (SENSE RDS(ON) )
3.
My use in condition is
VIN=5V
VOUT=0.95V
FSW=1.1M HZ
According to datasheet Figure 6 OCP is about 7.8A
Overcurrent limit on high-side FET=6.1/6.8/7.5A in the table by
to assess the minimum OCP 6.1/6.8=0.897
TYP=7.8A
MIN=7.8A*0.897=6.997A?
Hello Aaron,
1. You are right, I thought this was two different operating conditions for the same High-side FET current limit. My Bad.
3. I am not sure to understand what is the calculation you are doing here (ie. OCP 6.1/6.8=0.897). Could you elaborate ?
Thanks a lot!
Regards,
Dorian
Hi Dorian Brillet de Cande
Since I can't measure a lot, the minimum value of OCP under the conditions I use
But it can be known from Figure 6 that TYP is about 7.8A
In the table by the proportional relationship between MIN and TYP=6.1A/6.8A=0.897
Let's evaluate the minimum value of OCP under the conditions I use
7.8A * 0.897=6.997A?
Hello Aaron,
You can use this as a rule of thumb, I would expect some variation to this wild approximation.
Thanks,
Dorian