Hello,
Is it practical to parallel multiple TPS54260 outputs to get higher output current, like 10A? No information in the datasheet or the application notes found.
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If freewheeling diodes are used instead of SR (synchronous rectifier), outputs in parallel operation should be ok. If SR is used, the parallel will be in question and likely causing problem.
If using freewheeling diodes, although the parallel is ok, the current sharing ratio may not be 50%-50% if two in parallel, as there is no active current sharing mechnism based on the datasheet. The converters will share the load currents in sort of droop regulation which won't be able to make good sharing ratio and the ratio will be varying part to part and also varying with temperature change.
Now if 10A load is expected, more than four converters, at least five, will have to be in parallel as the current sharing ratio won't be 25% each if only four in parallel.