Hello,
Each TPS54260 chip can output a maximum current of 2.5A.
Is it practical to parallel multiple TPS54260 outputs to get higher current output capability, like 10A? Anyone has experience on this to share?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In general you can parallel devices that use current mode control. I have done this with the TPS54620 successfully (2 x 6 A = 12 A total). If you look in the product folder you will find documentation on this. I am not sure about putting more than 2 circuits in parallel. The layout is a little tricky even with 2 circuits as the shared portions are somewhat noise sensitive.