This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ7718: Need BQ771824 like device with 3.8V threshold OVP

Part Number: BQ7718
Other Parts Discussed in Thread: BQ77216, , BQ77207

Hi, 

my customer is looking for a device / solution similar to BQ771824 but with an OVP = 3.8V threshold. 

Is there anything we can recommend?

BR Josef 

  • Hi Josef,

    Our BQ7718 has a minimum OVP threshold of 3.85V. We have 2 devices, BQ77216 and BQ77207 that have the potential to support a 3.8V OVP. Currently, there are no versions with this threshold but we are working on more. We will add them to ti.com when they are finished, so keep checking back.

    Thanks,

    Shawn