This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2513: How to identify the charging device

Part Number: TPS2513

I would like to know the specific contents of DCP Auto-Detect.

How does the TPS2513 identify a compliant charging standard when a charging device is connected?

What does TPS2513 recognize and switch the following modes?

  • Ryousuke,

    The TPS2513 has a stat machine internal to the device that will check to see if any of the 3 divider modes or 1.2V short is present and then well execute the BC1.2 connection sequence.  This is a BC1.2 compliant connection sequence.

    Regards,

    Chuck