Hi,
I'm looking at replacing the TPS3710DDC(R/T) with an equivalent part in the same SOT23 package due to it being increasingly difficult to obtain the TPS3710 on Farnell, Digikey etc. (A broker sell this part for > $60 USD these days !)
Can somebody suggest an electrically equivalent, drop-in part in the SOT23 package, but with say, less input voltage range as this was never an important requirement to start with ...
An equivalent part with say 2V - 6V input voltage range (for battery voltages), that is stocked somewhere would do just fine.
Thanks in advance for your advice,
regards, MM