Hi sir,
We are using 5 PL455 in series and communicating with MCU ,Initially communication between PL455 and MCU is good but after few minutes we are not able to get the communication .
1. Which command should be used to reset the Communication request?
2. We have tried with the command mentioned in the Software Design file ,but the PL455A is not getting reset with the command provided.
3. Do we have to send any other baud rate etc along with communication reset request?
4. we also tried with auto addressing request but communication request is not happening?
Please help with the solution
Thanks
MV