This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z65-R1: Modify Full Charge Capacity of gas gauge for system testing

Part Number: BQ20Z65-R1
Other Parts Discussed in Thread: BQ20Z65

I'm trying to test a system error that detects high full charge capacity in a connected battery with the z65-R1 gas gauge. However, the error is triggered directly by reading a high FCC from the battery and comparing it to a constant, instead of checking the state of health. Since the system software cannot be modified, I need to modify a battery such that it erroneously reports a full charge capacity value that is approx. 1.5x the design capacity.

Can you suggest any parameters in the z65-R1 that I can modify to affect this change? Additionally, the change needs to be non-volatile, so that we can have a "modified" battery with which to perform this system test in the future. We had a battery like this in the past, but I don't remember what was changed to put it in that state.