Hello All,
We are working on a small peltier module control circuit : 3.8Vmax - 2Amax - 1.6Ohm
Atfer runing some lab tests, we reached a compromise in operational parameters with a maximum current of 800mA (hich is enough for our application). and since this would be supplied by a battery,the driving current must be limited.
Going through this application note : SLUA979A, It appears that constant current might be more efficient than PWM driving
and based on this : [FAQ] What motor drivers should be considered for driving Thermoelectric cooling (TEC) elements, or Peltier devices?. There are some pretty good drivers to use in such application. my issue is there either out of range of my requirements ( 3V - 0.8A) or currenlty out of stock.
I would appreciated if you can recommand any part number/application note compatble with this application
Thank you in advance for your support