Other Parts Discussed in Thread: LMR36015,
Will the switcher withstand a 202 V, 350 ms load dump if this is clamped to 60 V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Will the switcher withstand a 202 V, 350 ms load dump if this is clamped to 60 V?
???
Where does the 44 V come from? The datasheet says 4.5 V to 50 V.

and maximum rating 65 V.

That's why I ask if the LM34919C-Q1 can withstand a load dump 350 ms, clamped to 60 V.
PS: The one you suggested may suit my design, but it is out of stock and unknown when it will be available. The LM34919C-Q1 is in stock.
Hello
My mistake I was using the wrong data sheet.
The abs max for that device is 65V. So, your 60V pulse should be OK.
Thanks