We are constructing a circuit as shown below(please ignore the MAX4166 circuit on the left as we already isolated out from FemtoFET circuit).

VG1 is a function gen to generate a series of pulses to enable/disable FemtoFET while we are injecting a 50mV voltage through VS3, VF2 is where we probe the output.
When the signal frequency from VG1 <500kHz, the output waveform measured still within expectation. However, once the frequency getting higher than 500kHz, we start to see obvious spike from the waveform as shown in oscilloscope.
Even we construct another circuit and the SW is open, we also see some spikes coming out.

My question is,
- Is the spike we measured due to the high switching frequency at the gate? because in both cases we are inputting 5Mhz of signal to the FET.
- Do we have any femtoFET or FET which can handle higher frequency?