Other Parts Discussed in Thread: CSD97370Q5M, CSD97370AQ5M, CSD97374Q4M, CSD97376Q4M, CSD97394Q4M
Could you help to provide similar products that can replace CSD95379Q3M
Currently designed as TPS51623RSM+CSD95379Q3MT CPU: ,INTEL BRASWELL,N3160
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Could you help to provide similar products that can replace CSD95379Q3M
Currently designed as TPS51623RSM+CSD95379Q3MT CPU: ,INTEL BRASWELL,N3160
Hi,
We don't have other parts in the exact same package. Would different package be considered?
Then there might be many parts can be considered if package is flexible, you may go to the TI.com website to go through all power stages. The CSD95379 is just basic power stage without smart functions.
You may start with CSD95375/CSD95377, I am not sure which parts are available at this moment. You may go with higher current rating devices as well.
Hi Gareth,
CSD97370 has higher voltage rating, and without the SKIP# pin to select diode emulation mode/forced continuous conduction mode. Have you checked CSD95375/CSD95377 I recommended before? They are more similar to CSD95379 but higher current rating.
Hi Gareth,
Then you will need to review the datasheet specs with customer for those power stages, as the VDD POR/UVLO, PWM impedance/thresholds, etc, has some minor differences with CSD97370Q5M, CSD97370AQ5M. And depends on if they need SKIP# function, they may also check CSD95373A/372A, but again the spec has some difference, need customer to review the specs in details.
CSD95375/CSD95377 are simpler to use as replacement but I understand it's not available now.
Hi Gareth,
Those power stages have 30V voltage rating, so power loss might be slightly higher, but should be OK to use. If heavy load efficiency/thermal is concern then CSD97374 is better with higher current rating.