Hi,
For our internal project we are using TPS77818D LDO. Kindly review the attached schematics and let me know the comments.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
For our internal project we are using TPS77818D LDO. Kindly review the attached schematics and let me know the comments.

Hello,
I think the schematic looks fine. The schematic label indicates an input supply of 3.3V, but the title however suggests an Input supply voltage of 6V. An input supply voltage of 3.3V should not cause any issues, however, if a 6V input supply is being used, please take care to operate at an ambient temperature that ensures that the power dissipation does not take the Junction Temperature beyond 125ºC. Please also take care ensure that COUT (C20) has an ESR in the range 50mΩ ≤ RESR ≤ 1.5Ω. Thanks!
Regards,
Srikanth
Hello Shreehari,
May I know the reason for having the inductor at the Input of the LDO and what its value is? The inductor could cause voltage spikes during load transients and start-up. Increasing the value of the associated capacitor (C17) to 10uF e.g. would help reduce the magnitude of the spikes. Thanks!
Regards,
Srikanth
Hello Srikanth,
It is a Ferrite bead provided at input power. This is to filter the noise from the power.