Customer has a design with two TPS50601A-SP devices. The clocks are synchronized using the Master/Slave approach at 500 KHz, but each device outputs a different voltage. Can the devices be Enabled independently?
I believe this is OK. In the case where the Master is enabled, but the lave is not, the Master will still send out an inverted clock on the SYNC pin. The slave would have power (VIN/PVIN) but will not power up. In the case where the master is disabled, then the slave would operate with it's internal clock based on the RT resistor, which is set for 500 kHz. If the master is enabled with the slave already Enabled, the clock of the slave will eventually switch over to the inverted Master clock.
Any concerns we are overlooking?